Jambalaya
Jambalaya is traditionally a one pot dish, with a variety of meats and seafood, chopped vegetables and seasonings. Feel free to spice it up.
Servings
4
Ready In:
1 hour
Good For:
Main Dish
Jambalaya
By: Nelson Sosh
Ingredients
- 1 onion
- 1 bell pepper
- 1 clove garlic
- 1 pack of Andouille sausage
- 1 cup cooked chicken
- 2 cups jasmine or basmati rice
- Dash of Worcestershire sauce
- Dash of creole seasoning
Step by Step Instructions
Step 1
Chop and then sauté onion, pepper, garlic and sliced Andouille sausage in large pot until onions are clear.
Step 2
Add 2 cups jasmine or basmati rice, seasoning, and enough Worcestershire sauce until the rice is brown (no I don’t measure, usually about 1/4 of the bottle).
Stir together.
Step 3
Add 3 cups water, cooked chicken (I use baked chicken thighs or a rotisserie chicken with the skin taken off).
Stir again, put lid on pot, turn heat to medium low and cook for about 40-45 minutes until rice is cooked.
*If adding shrimp, don’t add until the last ten minutes. Cook until shrimp is pink. You can add a few more tablespoons water if needed.