PB & J
Have been enjoying this for many years. Even my grandmother served this.
Servings
1
Good For:
Lunch
Peanut Butter & Jelly aka PB&J
By: Eric Bombere

Ingredients
- 2 slices sandwich bread (white or wheat bread preferred, but gluten-free options available.)
- 2 to 3 oz. (1 or 2 Tbsp.) peanut butter (non-organic type suggested)
-
2 oz. (1 or 2 Tbsp.) jelly (grape preferred)
Advanced: slice the sandwich in half, diagonally
Step by Step Instructions
Step 1
Spread 1 oz. peanut butter on each slice of bread (one side each slice).
Step 2
Spread jelly on one of the slices (the side that has peanut butter).
Step 3
Put the 2 slices together so that the jelly on one slice faces the peanut butter on the other slice.