Cruciani’s Italian Spaghetti & Meatballs
This recipe was handed down from my Great Gramma, Mary Nesta. Gramma Nesta came to America from Italy in early 1900. Italian Spaghetti & Meatballs is our favorite dinner.
Ready In:
2 – 4 hrs
Good For:
Main Dish
Cruciani’s Italian Spaghetti & Meatballs
By: Mark Cruciani
Ingredients
Meatball Mix
- 3 lbs. of ground hamburger
- 1 lb. of ground pork
- 3/4 sleeve of saltine crackers (with or without salt)
- 3 whole eggs (break the eggs and add when you mix everything together)
- 3 tablespoons of sweet Basil
- 1 pinch of cayenne red pepper (more if you like it HOT – be careful though!)
- Onions (minced or diced)
Mix everything together. Then “hand roll”, making round meatballs. Broil meatballs in oven. Place in broiler, 9 minutes to start, turn meatballs over, 9 additional minutes.
Spaghetti Sauce
- 2 – 32 ounce cans of tomato juice
- 2 – 8 ounce cans of tomato paste (additional can of tomato paste if you like thick sauce)
- 3 tablespoons of sweet Basil
- 1 pinch of cayenne red pepper (more if you like it HOT – be careful though!)
Mix and add these sauce ingredients into a Slow Cooker.
Step by Step Instructions
Step 1
Once meatballs have been broiled, place them in the Slow Cooker with spaghetti sauce. Cook for as long as you like, but I recommend at least 2-4 hours before serving. You want to get the spices working!
Step 2
All you need now are your spaghetti noodles and you are ready for an Italian Feast! Enjoy from my family to yours.