Grandma Darlene’s Perogies
These savory filled dumplings are a weekly meal in Ukrainian country and when Grandma makes them, there’s no place like home.
Servings
Makes about 3 dozen
Ready In:
1.5 hours
Good For:
Main dish
Grandma Darlene’s Perogies
By: Maureen Stevenson
Ingredients
- 4-5 lbs boiled potatoes in salted water (save water)
- Butter
- Onions
- 4 cups cheddar cheese, grated
Dough
- 10 cups of flour
- 1 overflowing cup of oil
- 4 eggs
- 1 tsp salt
- 4.5 cups of potato water
Step by Step Instructions
Step 1
To make the filling:
Cook a pot of potatoes in salted water. Fry some butter and onions in a pan. When potatoes are done, drain and keep the water.
Mash the potatoes, and add the butter, onions and grated “old” cheddar cheese to taste.
Step 2
Crack eggs into bowl and add oil, whisk until mixed. Add the potato water. Mix in the flour until a soft dough is formed.
Let the dough rest a few minutes, then begin to roll it out on a floured surface. Roll it to a thickness of pie crust.
With a soup can, cut in circles.
Step 3
Place 1 1/2 teaspoons of filling on each round of dough. Gently fold the dough over, forming a pocket around the filling. Pinch the edges of the pierogi to seal, then seal again with the tines of a fork.
Step 4
At this point the pierogi can be frozen for up to 4 weeks, or refrigerated overnight, or cooked in a large stockpot of boiling salted water. Only cook about 10 pierogi at a time, so that they have room to float without sticking. When the pierogi float, they’re done. The time will vary depending on if they’re fresh or frozen.
Note: Bacon, cottage cheese or creamed cheese are great variations on the filling. Top with sour cream, onions fried in butter, or serve nacho style with salsa, cheese, and peppers.