Homemade Italian Bread
Ready In:
3 hours
Good For:
Bread & Rolls
Homemade Italian Bread
By: Dawn Robinson
Ingredients
- 3 cups flour
- 1 ½ Tbsp. sugar
- ½ Tbsp. salt
- 2 Tbsp. Oil (any kind)
- 1 package yeast (3 teaspoons)
- 1 ¼ cups water (lukewarm)
Step by Step Instructions
Step 1
Dissolve yeast in water. Let stand for at least 1-2 minutes.
Step 2
Add rest of the ingredients together. Stir yeast/water mixture and add to other ingredients. Mix thoroughly by hand or mixer. Knead bread by hand or in mixer for an additional 2-3 minutes until it forms a nice ball. I use a mixer then hand knead when it forms a ball.
Step 3
Place in a greased bowl and cover to rise for 1 hour. Spray the top with cooking oil when rising.
Step 4
Punch down dough and form into a loaf. Place in a greased loaf pan, cover and let rise 1 hour. Spray the top with cooking oil when rising.
Step 5
After risen, place bread in oven and bake for 20-25 minutes at 400°. Times may vary depending on the weather. You can tell when the bread is done by tapping lightly on the top. It will make a hollow sound.
Step 6
Let cool completely before slicing.
Optional
When done remove from oven and rub the top with butter. You can also sprinkle with herbs, parmesan cheese etc.