InstaPot Best Ever Beef Stroganoff
This is definitely a change of seasons family favorite!
Servings
6
Ready In:
41 minutes
Good For:
Main Dish
InstaPot Best Ever Stroganoff
By: Diane Clohesy

Ingredients
- 12 oz. package of wide ribbon-like egg noodles, boiled separately according to package (I find using half the package is enough but feel free to use it all)
- 1.5 – 2 lbs. of beef stew meat/chuck cubes OR chuck roast cut into cubes (NOT to be confused with cubed steak – AVOID that for this recipe. Make sure the cut you use is as marbled as possible with some fat on it as this will make for the most tender meat. Get a nice, marbled cut with visible, thick fat strands for the best experience.
- Kosher salt, a few generous shakes for seasoning the meat
- Black pepper, a few generous shakes for seasoning the meat
- 3 Tbsp. of olive oil
- 2 Tbsp. of salted butter
- 1 large yellow onion, diced
- 16 oz. of Baby Bella mushrooms, sliced (you can use 8 oz. instead if you want less mushrooms but I prefer it loaded with them)
- 1 Tbsp. of crushed garlic
- 1/4 cup of a dry white wine (like a Chardonnay or you can use white cooking wine)
- 1 Tbsp. of Dijon mustard (if you hate mustard, you won’t taste it. It simply brings out more flavor in the sauce once combined with the other ingredients)
- 1 tsp of seasoned salt
- 1.5 cups of beef broth (I use 2 tsp of bouillon + 1.5 cups of water)
- 1 teaspoon of dried thyme
- 2 Tbsp. of cornstarch + 2 Tbsp. of water
- 1 packet of dry onion dip/soup mix (like the kind you’d use for dips – there are many varieties and I used an Onion Mushroom flavor)
- 1 cup (8 oz.) of sour cream
- 5.2 oz. of a garlic & herb cheese spread (SECRET INGREDIENT! If you can’t find any garlic & herb cheese spread, which is usually located in the deli section of your supermarket, use 5 oz. of a brick of cream cheese)
Step by Step Instructions
Step 1
Cook the egg noodles on the stovetop according to package instructions; strain and set aside (Note: you can also do this during Step 7 while the Stroganoff is pressure cooking, but just make sure you do it separately on the stove and don’t add the noodles directly into the pot while pressure cooking or they will absorb too much of the liquid and will become mushy)
Step 2
Season the meat with the kosher salt & pepper (about 1-2 tsp of each should be fine) and rub it in well.
Step 3
Add the olive oil and butter to the Instant Pot and hit “Sauté” and adjust so it’s on the “More” or “High” setting.
After about 3 minutes (and once the butter’s melted and oil’s bubbling), add in the meat and sear on all sides so it’s lightly browned (about 2-3 minutes total; the meat shouldn’t be fully cooked at all). Remove the meat with a slotted spoon and place in bowl. Set aside.
Step 4
Next, add in the white wine and stir for a minute followed by the dijon mustard and seasoned salt, stir well and deglaze (scrape) the bottom of the pot so nothing’s stuck to it.
Step 5
Lastly, add in the beef broth and thyme and stir well followed by adding back in the browned beef.
Step 6
Secure the lid, hit the “Keep Warm/Cancel” button followed by the “Manual” or “Pressure Cook” button High Pressure for 7 minutes for firmer meat and 12 minutes for more tender meat. Do a quick release when done OR allow a 10 minute natural release (meaning you do nothing for 10 minutes when done and the timer count up to either “00:10” or “L0:10”) followed by a quick release if you wish it to be more tender – this goes for either cooking time you choose.
Step 7
When the lid comes off, hit the “Keep Warm/Cancel” button and then hit “Sauté” again and adjust so it’s on the “More” or “High” setting.
Bring the pot to a bubble and add in the cornstarch slurry and stir immediately. Then, add in the onion mix packet and let bubble for a minute and then turn the pot to “Keep Warm” so that the bubbles die down.
Step 8
Once the bubbles have mostly subsided, add in the sour cream and cheese spread. Stir well until they are both totally melded into the sauce and it will be ready!
Place some noodles in individual bowls and then follow with some the beef and plenty of sauce. Enjoy.