Joyce’s Sweet Potato Casserole
If you’re looking for a healthy version of sweet potatoes, this is not it. But it’s delicious!!!
Good For:
Side Dish
By: Christie Kiefer
Joyce is my Mama, and this is one of her signature southern dishes. It is present at all holiday meals and many church and civic functions.
Ingredients
- 3 cups sweet potatoes, boiled and mashed
- 1 cup sugar
- 1/2 cup butter
- 2 large eggs, beaten
- 1/3 cup milk
Topping:
- 1 cup brown sugar, packed
- 1/2 cup flour
- 1/3 cup butter, melted
- 1 cup pecans, chopped
Step by Step Instructions
Step 1
Combine boiled and mashed sweet potatoes with sugar, butter, beaten eggs and milk. Pour into casserole dish. Set aside. (Note: I boil potatoes whole and still in the skin to retain flavor and moisture. Also, peeling cooked skin is much easier to remove than peeling raw potatoes.)
Step 2
For the Topping:
Combine brown sugar, flour, butter and pecans. Sprinkle on top of sweet potato mixture.
Step 3
If cooking immediately, place in preheated 350 degree oven for 30 to 35 minutes or until topping is brown and/or casserole is bubbly.
Step 4
If not baking immediately, store in refrigerator. Add cooking time of 15 to 20 minutes if baking cold casserole. (Place cold casserole dish in cold oven to prevent dish from breaking.)