Strawberry Dream
My kids’ favorite dessert because they love strawberries. You can also use kiwi, raspberries, peaches or any other juicy fruit you like. The cream can also be used to translate the layers of the cake.
Servings
6
Ready In:
1hr 30min
Good For:
Dessert
Strawberry Dream
By: Monika Rzepka
Ingredients
- 100 grams of white chocolate
- 250 grams mascarpone cheese
- 250 grams cream 30-36% of fat
- 500 grams of strawberries (fresh or frozen, frozen should be defrosted)
-
200 grams of granola
Step by Step Instructions
Step 1
The evening before, boil the cream in a pot and put the broken chocolate into it. Stir vigorously until the chocolate is completely melted. After it has cooled down, put it in the refrigerator overnight.
Step 2
The next day, beat the cold cream and chocolate with a mixer together with the mascarpone cheese to a stiff cream.
Dice the strawberries.
Step 3
For low glasses, alternate layers: granola, cream, strawberries until the glass is full. Garnish with a mint leaf and serve.