Voter Family’s Baby Back Ribs
Enjoy these tender ribs with a rub that has taken our family years to perfect. Some folks like to eat them straight off the grill, but if you want them extra tender/falling off bone, the secret is to put the BBQ sauce on, wrap in foil, and cook for another hour or so.
Ready In:
Overnight
Good For:
Main Dish
Voter Family’s Baby Back Ribs
By: Lynsey Voter
Ingredients
Rib Rub (enough for 3 racks):
- 2 cups brown sugar
- 1/2 cup kosher salt
- 1/4 cup paprika
- 1/4 cup steak seasoning
- 1/4 cup garlic powder
- 1 Tbsp. ground pepper
- 1 tsp. dried basil
- 1 tsp. thyme
- 1 tsp. cayenne
Step by Step Instructions
Step 1
Mix Rib Rub together.
Rub on ribs, cover and refrigerate overnight.
Step 2
Preheat oven to 300 degrees. Double wrap in foil, so no air can escape. Bake at 300 for 2 hours and 15 min.
Step 3
Unwrap from foil and BBQ on medium for 20 min (or until desired char).
Step 4
Smother with your favorite BBQ sauce and re-wrap in foil. Put back in oven at 175 degrees for at least 1 hour.