Zucchini Nut Muffins
I usually double, or even quadruple this recipe, as it seems to disappear fast in my family. It has been a tradition for almost two decades. In the summer, it’s just fun to go pick fresh zucchini from the garden, and make a mess baking in the kitchen.
Servings
1 loaf or 12 muffins
Ready In:
1 hour
Good For:
Bread & Rolls
Zucchini Nut Muffins
By: Bob Lupica
Ingredients
- 1 1/2 cups all purpose flour
- 1 teaspoon ground cinnamon
- 1/2 teaspoon baking soda
- 1/2 teaspoon salt
- 1/2 teaspoon ground nutmeg
- 1/4 teaspoon baking powder
- 1 cup sugar
- 1 cup shredded “unpeeled” zucchini
- 1 egg
- 1/4 cup cooking oil
- 1/4 teaspoon shredded lemon peel (lemon spice or orange spice works well too)
- 1/2 cup chopped walnuts (optional)
Step by Step Instructions
Step 1
Preheat oven to 350 degrees.
Mix together flour, cinnamon, baking soda, salt, nutmeg, and baking powder in a separate bowl.
Step 2
Using a different bowl, combine shredded zucchini, sugar, egg, oil, and lemon peel. Mix well.
Step 3
Stir in the flour mixture from step 1, then add the walnuts (optional).
Step 4
Pour batter into a bread loaf pan, muffin tins, or whatever shape you want. Even though it is more work, I like to to use “mini” muffin pans. Great for a quick snack.
Step 5
Depending on the batch size, baking time will very greatly. Full loaves may take up to 1 hour, and mini muffins may take just 12 minutes.
Just use a toothpick to to poke into it, and when it comes out clean, it’s done. Enjoy!